Energy Efficiency

Success Story: Water

Bacviz Kecskemet (Hungary)

Service solution to reduce energy consumption and electricity bill in a pumping station

Success Story: Water 15%  energy savings, ROI in less than 3 years

 

I. CUSTOMER ENVIRONMENT / PROJECT CONTEXT

 

Customer profile:

  • Bacviz is the operation company in charge of providing drinking water to the town and region of Kecskemet. It represents a population of 120 000 inhabitants.
 

Customer objective and constraints:

  • In Hungary the electrical utility providing electrical energy to the water operation company has a price policy based on a fixed subscription. When the water utility has peak demands over the subscription value some penalties are applied. The water utility, want to avoid this cost.
  • More generally a clear understanding of the consumption of the different process steps is required to optimize the process. On average electricity bill represents up to 30% of operation cost for a water utility.
 

II. SOLUTION IMPLEMENTATION

 

Implementation methodology (main phases):

1. Meeting with operators to understand the key step of its process : deep underground pumping, sand filters, chlorination.
2. Instrumentation of the electrical network of the customer with measurement devices connected to a web server.
3. Analysis of the data collected by the Schneider Electric services team.
4. Creation of an official report on a regular basis and presentation of the conclusions to the operation company staff.
 

Duration:

  • 2 years: 2004 to 2006
 

Solution overview (services, products, systems, architectures...):

 
Solution overview (services, products, systems, architectures...):1. Revamping of Low Voltage switchgear
2. Compact NS Micrologic electronic trip units
3. Powerlogic meters and control
4. Modbus/Ethernet communication units
5. Ethernet server information collection
6. Information analysis
 

How did we estimate the energy savings (methodology, tools, ...)

  • Energy savings have been directly obtained by the reduction of the contract from a 600kW base to a 400kW base (winter subscription)
 

III. RESULTS / ACHIEVEMENT

 

Customer benefits:

  • The customer has a lower contract with the water utility.
  • He is able to manage the process to avoid peak demand : no filters backwashing during deep water pumping for instance.
  • Balancing of the pumps to limit ageing.
  • Pulsed air compressor optimisation.
 

Customer testimonies (Verbatim):

  • Plant operation manager: "After 6 months of operation and the two first monitoring reports we have optimized the energy cost . We wish to extend the complete supervision of our electrical equipment on 2 pumping stations at Kecskemet."
 

Schneider Electric differentiating values VS competitors:

  • Local service team collaboration with a local panel builder.
  • Full solution proposed by the same team including electrical equipment revamping, Ethernet TCP/IP transmission of data via a safe router, interpretation of data by experts, quarterly reports for recommendations.
 
 
 
 

To know more 

Requests for Solutions, Products and Services information

Contact your Customer Care Centre now!
 

Solution breakdown

Main services:
  • Engineering services: Services
Main products & systems:
  • Compact NS
  • Powerlogic
  • Variable speed drive ATV