Retail
Success Story: RetailCity's Nisantasi Life-Style Center, Istanbul (Turkey)Building solutions with a metering advantage![]() I. CUSTOMER ENVIRONMENT / PROJECT CONTEXTCustomer profile:City's Nisantasi Life-Style Center is located on the street of Tesvikiye which is the heart of shopping in the luxurious district of Nisantasi, Istanbul. It is more of a life-style center than a shopping mall as it converges art and fashion in the most prestigious location of the city, with its architectural conformity of the historical and cultural structure of the region.City's features 150 stores, 9 cinema theatres, a 6 storey car-park, glocal brands, cafes and exclusive restaurants Customer objective and constraints:City's Nisantasi project is a prominent A+ project that has the top location in Istanbul with an investment of US$ 125,000,000. The client behind this venture was Gülaylar group, a jewellery ad luxury goods retailer, who was building their first shopping mallThe client wanted tenant metering for each of its shop owners based on W.A.G.E.S. and energy metering/ monitoring as part of the solution offer which would later conclude as energy optimization II. SOLUTION IMPLEMENTATIONImplementation methodology (main phases):Phase 1: Schneider Electric offered an energy consultancy role to study the various requirements of the client (Gülaylar) and their tenants. This included, understanding various lighting needs in accordance with store design formats and air quality needs in accordance with goods sold
Phase 2: An integrated HVAC and Lighting Control solution was implemented in an open architecture (LonWorks) to a single end BMS Workstation for facility management. Air Quality monitoring and control was further integrated for car-park and mall vicinities to ensure customer comfort Phase 3: A metering strategy was studied and installed for City's Nisantasi with a view to have tenant metering over a W.A.G.E.S portfolio. This included VRV (Variable Refrigerant Volume) monitoring through special meters, alongside electricity and water. A proprietary invoicing software was made by SE Turkey based on the clients requirements. This software allowed for the inputs from HVAC (Daikin VRV system) to be converged with Water and Electricity usage details and tariff, and finally displayed on a common accounting interface. Phase 4: Medium Voltage power protection solutions was installed and the output fed to the BMS workstation. Schneider Electric also helped address a customised load shedding solution for City's in the eventuality of a power shortage or outage. This mechanism is controlled by SCADA and fed by Modbus into the BMS. Hence making a seamless crosslink between Power and BMS. Phase 5 included tying all the energy information outputs to the BMS workstation for an integrated database management, hence the mall was able to charge its tenants for justified consumptions. Phase 6 took energy management further with an all-round facility management offer ![]() Solution overview (services, products, systems, architectures...):![]() III. RESULTS / ACHIEVEMENTCustomer benefits:Schneider Electric was able to assist City's Nisantasi with a modular offer by which they could build on their energy management strategy and key elements on a step-by-step approachWith a customised metering strategy and a tenant-oriented tariff workflow processed through the BMS workstation, the mall could do real-time analysis and overview of its energy consumptions and hence reduce operating costs. By having all metering and BMS functions processed through LonWorks, the mall was also allowed flexibility in its choice of operations for long-term and the facility managers were given the benefit of having an IP oriented control over all measurement parameters.
Solution breakdownMain services:
|