Hotels
Success Story: HotelsHotel facility "U Hájků" (Czech Republic)3 hotels, passage and congress centre![]() I. CUSTOMER ENVIRONMENT / PROJECT CONTEXTCustomer profile:
Customer objective and constraints:The investor wanted one company, which would be able to supply all electrical systems as one package. They also wanted high energy efficiency of the entire facility and the capacity to drive the complete installation from a central point.II. SOLUTION IMPLEMENTATIONImplementation methodology (main phases):The complete project was divided into 4 parts. The first part includes the congress centre and shopping mall. The three other parts represent each of the three hotels.Schneider Electric implemented turn-key solutions including third party systems like audio system, Cisco active components, radio etc. Solution overview (services, products, systems, architectures...):![]() Building Management System functionalities:
How did we estimate the energy savings (methodology, tools, ...)The monitoring & control of the complete installation allows an optimized management of all the systems and allows importnat energy savings.Load shedding and contract negociation with the electrical supplier had an immediate impact on the energy bill. III. RESULTS / ACHIEVEMENTCustomer benefits:The provided solution allows the customer to drive and optimize its installation from a single point of control. He can also access all the information remotely through a Web server.The integration of electrometers and heat meters into the control system ensures the follow-up of energy consumptions of individual tenants. Load shedding capabilities in case of pick cunsumptions is one of the key function to avoid additional energy cost. Thanks to the clear visibility of the energy consmptions, the best contract can be negociated with the energy supplier.
Solution breakdown
|