System Integrators dedicated area
UAG – Unity Application GeneratorUnity Application Generator is an advanced design and generation software tool that integrates multiple PLCs and HMI/SCADA systems to provide an automation solution similar to a Distributed Control System. UAG- An Innovative Software
An Advanced Automation PlatformUAG integrates best in class products from Schneider Electric and leading partners into an advanced automation platform based on standards including ISA-88, GAMP, IEC61131-3:
UAG Success Stories
Benefits of using the Unity Application Generator, to System Integrators:
For the process engineer, Unity Application Generator allows the user:
For the control engineer, Unity Application Generator allows the user:
|