Consultants & Designers
News:Discover the Energy Efficiency solution of the week and receive for free the catalogue of 35 solutionsThe most energy efficient way to control air-water exchange in a cooling tower is to use a variable speed drive for the fan and a variable speed drive for the pump. This application with speed drive uses up to 50% less energy than pump and fan direct-start and eases maintenance.
This solution is part of a set of HVAC control application sheets. In this chapter, you will see how HVAC energy consumption levels can be reduced by improving the control and management of ventilation, temperatures, and system usage, with speed drive and motor starter.
You can find more energy efficiency solutions for buildings in a 35-solutions catalogue with Schneider Electric products combination.
> Register to receive the complete pdf catalogue of 35 solutions for energy efficiency in buildings.
|